2019-10-24 9:05 AM
Hi,
So I am trying to use the example of "FDCAN_Classic_Frame_Networking" from the mentioned examples in other thread STM32Cube_FW_H7_V1.2.0\Projects\STM32H743I_EVAL\Examples\FDCAN\FDCAN_Classic_Frame_Networking
But I am always caught in an error when initializing the HW. I am debugging to see exactly where it stops and it happen to be in initialization and specifically a timeout in these lines
// File is stm32h7xx_hal_fdcan.c
// lines 310 and 311
/* Wait until the INIT bit into CCCR register is set */
while((hfdcan->Instance->CCCR & FDCAN_CCCR_INIT) == RESET)All my settings are as in the example, but it never set that bit in the register to continue.
Have you encountered something similar or know a way to solve this issue?
Thanks in advance.
2019-10-31 8:23 AM
I have solved the problem now.
My problem was that I needed to specify the communication parameters in the STM32CUBEIDE and get the timing parameters from http://www.bittiming.can-wiki.info/ specifiying the brand , clock speed and CAN speed.
Everything is working now, and the example is too.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.