2011-07-10 9:33 PM
Is this on a board you created, or a commercial eval board?
this is the board created not a commercial eval board, I also have a commercial board on which it is working perfect.Check the wiring, and connection, of the JTAG port?Wiring and connection are proper.Check if you want to use SWD vs JTAG signalling. I wanted JTAG, but both are not working Check you have current drivers and firmware from SEGGER.
As it is working on the eval board properly, I feel drivers are installed properly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.