cancel
Showing results for 
Search instead for 
Did you mean: 

Failture to start motor with stm32f0 and mc33926

pemo nowak
Associate
Posted on November 25, 2017 at 12:54

Hello,

I have problem to start motor with sm32f0 and single motor driver mc33926. I was in pololu forum and they sad that everything connection is ok, but still dont work. I have joystick to control speed motor. Adc reading it's ok, I check this in stmstudio. Please, help me

&sharpinclude <stm32f0xx_gpio.h>

&sharpinclude <stm32f0xx_rcc.h>

&sharpinclude 'stm32f0xx_adc.h'

&sharpinclude 'stm32f0xx_tim.h'

GPIO_InitTypeDef Gp;

ADC_InitTypeDef ADC_INIT;

TIM_TimeBaseInitTypeDef timerInitStructure;

TIM_OCInitTypeDef outputChannelInit;

&sharpdefine GreenLED_Pin GPIO_Pin_9

&sharpdefine BlueLED_Pin GPIO_Pin_8

&sharpdefine przycisk_Pin GPIO_Pin_0

int odczyt_adc;

int i;

uint8_t ButtonRead = 0;

uint8_t blad = 1;

&sharpdefine IN2 GPIO_Pin_14 //PB14

&sharpdefine IN1 GPIO_Pin_13 //PB13

&sharpdefine EN_P GPIO_Pin_6 //PC6

&sharpdefine SLEW GPIO_Pin_7 //PC7

&sharpdefine SF_pin GPIO_Pin_7 //PA7

&sharpdefine PWM_pin GPIO_Pin_3 //PA3

void wyjscia_init(void)

{

      Gp.GPIO_Pin =GreenLED_Pin | BlueLED_Pin | EN_P | SLEW;

      Gp.GPIO_Mode = GPIO_Mode_OUT;

      Gp.GPIO_OType = GPIO_OType_PP;

      Gp.GPIO_PuPd = GPIO_PuPd_NOPULL;

      Gp.GPIO_Speed = GPIO_Speed_Level_1;

      GPIO_Init(GPIOC, &Gp);

      Gp.GPIO_Pin = IN1 | IN2;

      Gp.GPIO_Mode = GPIO_Mode_OUT;

      Gp.GPIO_OType = GPIO_OType_PP;

      Gp.GPIO_PuPd = GPIO_PuPd_NOPULL;

      Gp.GPIO_Speed = GPIO_Speed_Level_1;

      GPIO_Init(GPIOB, &Gp);

}

void wejscia_init(void)

{

      Gp.GPIO_Pin = SF_pin | przycisk_Pin;

      Gp.GPIO_Mode = GPIO_Mode_IN;

      Gp.GPIO_PuPd = GPIO_PuPd_NOPULL;

      GPIO_Init(GPIOA, &Gp);

}

void ADC_init(void)

{

        ADC_DeInit(ADC1);

        Gp.GPIO_Mode = GPIO_Mode_AN;

        Gp.GPIO_OType = GPIO_OType_PP;

        Gp.GPIO_Pin = GPIO_Pin_1;

        Gp.GPIO_PuPd = GPIO_PuPd_NOPULL;

        Gp.GPIO_Speed = GPIO_Speed_50MHz;

        GPIO_Init(GPIOA,&Gp);

        ADC_INIT.ADC_Resolution = ADC_Resolution_12b;

        ADC_INIT.ADC_ContinuousConvMode = ENABLE;

        ADC_INIT.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

        ADC_INIT.ADC_DataAlign = ADC_DataAlign_Right;

        ADC_INIT.ADC_ScanDirection = ADC_ScanDirection_Upward;

        ADC_Init(ADC1, &ADC_INIT);

        ADC_Cmd(ADC1, ENABLE);

        ADC_ChannelConfig(ADC1,ADC_Channel_1, ADC_SampleTime_71_5Cycles);

        ADC_StartOfConversion(ADC1);

}

void PWM_INIT(void)

{

            Gp.GPIO_Pin = PWM_pin;

            Gp.GPIO_Mode = GPIO_Mode_AF;

            Gp.GPIO_OType = GPIO_OType_PP;

            Gp.GPIO_PuPd = GPIO_PuPd_NOPULL;

            Gp.GPIO_Speed = GPIO_Speed_50MHz;

            GPIO_Init(GPIOA,&Gp);

            GPIO_PinAFConfig(GPIOA, PWM_pin, GPIO_AF_2);

            timerInitStructure.TIM_Prescaler = 48000;

            timerInitStructure.TIM_CounterMode = TIM_CounterMode_Up;

            timerInitStructure.TIM_Period = 4000;

            timerInitStructure.TIM_ClockDivision = TIM_CKD_DIV1;

            timerInitStructure.TIM_RepetitionCounter = 0;

            TIM_TimeBaseInit(TIM2, &timerInitStructure);

            outputChannelInit.TIM_OCMode = TIM_OCMode_PWM1;

            outputChannelInit.TIM_OutputState = TIM_OutputState_Enable;

            outputChannelInit.TIM_Pulse =3000;

            outputChannelInit.TIM_OCPolarity = TIM_OCPolarity_High;

            TIM_OC4Init(TIM2, &outputChannelInit);

            TIM_OC4PreloadConfig(TIM2, TIM_OCPreload_Enable);

            TIM_Cmd(TIM2, ENABLE);

}

int main(void)

{

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

  wyjscia_init();

  wejscia_init();

  ADC_init();

  PWM_INIT();

  while(1)

  {

    GPIO_SetBits(GPIOB, IN1);

     GPIO_ResetBits(GPIOB, IN2);

     GPIO_SetBits(GPIOC, EN_P);

     GPIO_SetBits(GPIOC, SLEW);

  odczyt_adc=ADC_GetConversionValue(ADC1);

  TIM_SetCompare1(TIM2,odczyt_adc);

  ButtonRead = GPIO_ReadInputDataBit(GPIOA, przycisk_Pin);

  blad = GPIO_ReadInputDataBit(GPIOA, SF_pin);

if(ButtonRead)

     GPIO_SetBits(GPIOC, GreenLED_Pin);

if(blad)

{

     GPIO_SetBits(GPIOC, BlueLED_Pin);

     for(i=0;i<1000000;i++);

     GPIO_ResetBits(GPIOC, BlueLED_Pin);

     for(i=0;i<1000000;i++);

}

  }

 }

#pwm-stm32f0 #pwm
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.