2008-08-06 11:12 PM
Failed to load flash loader_ADC-DMA:STM3210B-Eval
2011-05-17 3:41 AM
Hello everyone
I have a very peculiar problem after programming (Flash) my STM3210B-Eval board. I first tried using an example program and it was programmed into the controller successfully (tried it many times with various modifications). I then tried programming the ADC-DMA functionality and for the ''first time'' the programming was successful, but after that, everytime when I try to debug any program (with/without ADC-DMA), I get this log - showing flash loader error Thu Aug 07 13:02:11 2008: DLL version: V3.72a, compiled Jun 18 2007 18:58:11 Thu Aug 07 13:02:11 2008: Firmware: J-Link ARM V6 compiled Jun 14 2007 14:33:17 Thu Aug 07 13:02:11 2008: JTAG speed is initially set to: 32 kHz Thu Aug 07 13:02:11 2008: Found Cortex-M3, Little endian. Thu Aug 07 13:02:12 2008: TPIU fitted. Thu Aug 07 13:02:12 2008: FPUnit: 6 code (BP) slots and 2 literal slots Thu Aug 07 13:02:12 2008: Software reset was performed Thu Aug 07 13:02:12 2008: Initial reset was performed Thu Aug 07 13:02:12 2008: J-Link found 2 JTAG devices. ARM core Id: 3BA00477(Cortex M3), ARM core Id: 00000000(ARM9) Thu Aug 07 13:02:12 2008: Device at TAP0 selected Thu Aug 07 13:02:12 2008: 3518 bytes downloaded and verified (5.65 Kbytes/sec) Thu Aug 07 13:02:12 2008: Warning: Verify error at address 0x2000011C, target byte: 0xD4, byte in file: 0x00 Thu Aug 07 13:02:12 2008: Warning: Verify error at address 0x2000011D, target byte: 0x08, byte in file: 0x68 Thu Aug 07 13:02:12 2008: There were warnings during download of FLASH loader, see Log Window Thu Aug 07 13:02:15 2008: Failed to load flash loader: C:\Program Files\IAR Systems\Embedded Workbench 4.0 Kickstart\arm\config\flashloader\ST\FlashSTM32F10x.d79 Additionally I tried to program another EVAL board with the example program (without ADC-DMA) and there are no errors. All that I have understood is there is some problem after programming the ADC functionality, but not able to resolve it. Kindly help me in this regard Thanks AR2011-05-17 3:41 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.