2014-11-13 1:19 AM
I'm using USB HS host mode with internal PHY but get a problem that i can't enter the interrupt when i plug or unplug my usb device. my program code is modified from host_device_libV2.10-USB_host_example. i just modified some init code:
i already defined USE_EMBEDDED_PHY marco and there are init code:
USBH_Init(&USB_OTG_Host,
USB_OTG_HS_CORE_ID,
&USB_Host,
&USBH_MSC_cb,
&USR_Callbacks);
void USB_OTG_BSP_Init(USB_OTG_CORE_HANDLE *pdev)
{
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOB , ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15 |
GPIO_Pin_14;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOB,GPIO_PinSource15,GPIO_AF_OTG2_FS) ;
GPIO_PinAFConfig(GPIOB,GPIO_PinSource14,GPIO_AF_OTG2_FS) ;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_OTG_HS, ENABLE) ;
}
2014-11-13 8:25 AM
Make sure USE_USB_OTG_HS is defined, and that you're using the right IRQ
NVIC_InitStructure.NVIC_IRQChannel = OTG_HS_IRQn; #ifdef USE_USB_OTG_HS void OTG_HS_IRQHandler(void) { USBD_OTG_ISR_Handler (&USB_OTG_dev); } #endif The example code also uses PB12 (OTG_HS_ID) and PB13 (OTG_HS_VBUS) RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB , ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOB,GPIO_PinSource12, GPIO_AF_OTG2_FS); GPIO_PinAFConfig(GPIOB,GPIO_PinSource14, GPIO_AF_OTG2_FS); GPIO_PinAFConfig(GPIOB,GPIO_PinSource15, GPIO_AF_OTG2_FS); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_Init(GPIOB, &GPIO_InitStructure); RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_OTG_HS, ENABLE) ; # global definitions for C++, C and ASM (e.g. ''symbol_with_value=0xDEAD symbol_without_value'') GLOBAL_DEFS = USE_STDPERIPH_DRIVER STM32F429_439xx USE_STM32F429I_DISCO USE_USB_OTG_HS USE_EMBEDDED_PHY HSE_VALUE=8000000We’re moving the ST Community to a new platform to give you a better and more reliable community experience.