2015-12-25 4:55 PM
I am using the USART1 interface of an F103 and I'm havin trouble getting interrupts correctly. When receiving a byte the first interrupts get triggered while bit 6 is still underway and then a second interrupt happens for some unknown reason.
row1 is debug pin that is being toggled ever irqrow2 is rx pinrow3 is tx pinvoid USART1_Init(void){ /* USART configuration structure for USART1 */ USART_InitTypeDef usart1_init_struct; /* Bit configuration structure for GPIOA PIN9 and PIN10 */ GPIO_InitTypeDef gpioa_init_struct; /* Enalbe clock for USART1, AFIO and GPIOA */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1 | RCC_APB2Periph_AFIO | RCC_APB2Periph_GPIOA, ENABLE); /* GPIOA PIN9 alternative function Tx */ gpioa_init_struct.GPIO_Pin = GPIO_Pin_9; gpioa_init_struct.GPIO_Speed = GPIO_Speed_50MHz; gpioa_init_struct.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &gpioa_init_struct); /* GPIOA PIN9 alternative function Rx */ gpioa_init_struct.GPIO_Pin = GPIO_Pin_10; gpioa_init_struct.GPIO_Speed = GPIO_Speed_50MHz; gpioa_init_struct.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &gpioa_init_struct); /* Baud rate 9600, 8-bit data, One stop bit * No parity, Do both Rx and Tx, No HW flow control */ usart1_init_struct.USART_BaudRate = 9600; usart1_init_struct.USART_WordLength = USART_WordLength_8b; usart1_init_struct.USART_StopBits = USART_StopBits_1; usart1_init_struct.USART_Parity = USART_Parity_No ; usart1_init_struct.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; usart1_init_struct.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_Init(USART1, &usart1_init_struct); /* Enable RXNE interrupt */ USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); NVIC_InitTypeDef NVIC_InitStructure; NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Enable USART1 global interrupt */ NVIC_EnableIRQ(USART1_IRQn); /* Enable USART1 */ USART_Cmd(USART1, ENABLE);}void USART1_IRQHandler(void){ static int tx_index = 0; static int rx_index = 0; static char rx_byte; if(USART_GetITStatus(USART1, USART_IT_RXNE)) { rx_byte=USART1->DR; if(rx_byte != 'x') { USART_SendData(USART1, rx_byte); } /*telemetry_rx_buffer[rx_index++] = USART_ReceiveData(USART1); if (rx_index >= (sizeof(telemetry_rx_buffer) - 1)) rx_index = 0;*/ debugpin_cycle(); }}What am i doing wrong here? #stm32-f1-usart-uart-problem2015-12-25 5:14 PM
What am i doing wrong here?
debugpin_cycle(); // infers something different than toggling, code not shown
2015-12-26 1:53 AM
Here's what debugpin is about:
void debugpin_init(void){ GPIO_InitTypeDef GPIO_InitStructure; //configure pin as output GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOB, &GPIO_InitStructure);}void debugpin_set(int value){ GPIO_WriteBit(GPIOB, GPIO_Pin_1, !value);}void debugpin_cycle(void){ GPIO_WriteBit(GPIOB, GPIO_Pin_1, 1); GPIO_WriteBit(GPIOB, GPIO_Pin_1, 0);}2015-12-27 3:56 AM
Fuck me, i was uploading release when working on debug. That's why nothing seemed to fix it. It now works great.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.