2018-07-05 5:49 AM
Diving into STM32F091 Nucleo Examples (STM32Cube_FW_F0_V1.9.0).
Trying ADC Sequencer and find this comment in main.c:
#if defined(WAVEFORM_VOLTAGE_GENERATION_FOR_TEST)
/** * @brief For this example, generate a waveform voltage on a spare DAC * channel, so user has just to connect a wire between DAC channel * (pin PA.04) and ADC channel (pin PA.04) to run this example. * (this prevents the user from resorting to an external signal generator) * This function configures the DAC and generates a constant voltage of Vdda/2. * To modify the voltage level, use function 'WaveformVoltageGenerationForTest_Update' * @param None * @retval None */static void WaveformVoltageGenerationForTest_Config(void)Besides being unable to connect PA4 with PA4 (DACOUT1 and ANIN4 are both at PA4), two questions:
- Is there any detailed structure doc of e.g. STM32F091 pin PA4 (AIN4 and DACOUT1) regarding ADC and DAC ?- Is it possible to read a DAC back via AIN if they share the same pin (PA4 in my case)?
Juergen
2018-07-05 6:16 AM
[CubeF0]\Projects\STM32F091RC-Nucleo\Examples\ADC\ADC_Sequencer\readme.txt says:
If ADC channel and DAC channel are selected on the same GPIO (default configuration
in this example): connection is done internally in GPIO pad, user has nothing to connect.JW
2018-07-05 11:06 PM
This should go into the Reference Manual...
2018-07-06 2:02 AM
Wholeheartedly agree.
The STM32s came to be in the same way as all modern highly integrated digital electronics does: by stitching together modules. The RM reflects this, leaving the &39stitches&39 (i.e. the places where modules interact closely or have direct (other than through the bus system) mutual connections) described rather weakly.
In newer STM32s&39 RMs (e.g. the &39L4) there&39s an Interconnection chapter, even if those still leave many important issues unaddressed - e.g. I doubt such ADC-DAC interaction or
https://community.st.com/0D50X00009XkaBBSAZ
interactionhttps://community.st.com/0D50X00009XkVvOSAV
beyond the GPIO module is mentioned in any of them. I was already suggesting here several times to put this into the older families&39 RMs too.JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.