2015-09-11 4:23 AM
Hi ,
I'm using STM32F103 and i have an input signal on Timer1_ch3 (PA10) which generates an EXTI interrupt and it's working well.I have another input signal on Timer2_ch3, but something strange happens when i connect this signal on the default Timer2_ch3 pin (PA2),it affects the EXTI interrupt and it becomes generated twice : one time like previous with the first signal and second time with the falling edge of the second signal!!!but when i avoid PA2 and remap the Timer2_ch3 on PB10 it works well. i can't understand why and i need to use PA2. void Init(void) { GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 ; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_PinRemapConfig(GPIO_FullRemap_TIM2, ENABLE); /* GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 ; // if i use PA2 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); */ GPIO_EXTILineConfig(GPIO_PortSourceGPIOA, GPIO_PinSource10); EXTI_InitStructure.EXTI_Line = EXTI_Line10; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); NVIC_InitStructure.NVIC_IRQChannel = EXTI15_10_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.