2013-04-19 1:50 AM
Hello,
I've doubts regarding
the access of an external SRAM (IS61WV102416BLL) connected to the FSMC bus that has the following spe
cifications
. This SRAM is organized as 1024K
x 16-bit
.
My assumption is,
by using the following code (SRAM is mapped to
0x
64000000)
, I would be able toaccess t
wo consecutive
half-words (16-bit wide)
:
1.
volatile
uint16_t * p_sram_1 = (
volatile
uint16_t *)0x64000000;
2.
volatile
uint16_t * p_sram_2 = (
volatile
uint16_t *)0x64000001;
3.
4.
*p_sram_1 = 0xBBAA;
5.
*p_sram_2 = 0xDDCC;
6.
7.
uint16_t data1 = *p_sram_1;
8.
uint16_t data2 = *p_sram_2;
I expect t
hat data1
w
ill contain
0xBBAA and data2, 0xDDCC
. But when I execute this code, data1 contains
0xCCAA
instead of 0xBBAA. This let me think that each address accesses one byte
instead of two bytes that I expected.
Am I totally wrong with my expectations or is
the FMS
C
bus translating unalign
ed addresses accesses in upper byte or lower byte access
es?
Thank you for your help.
#external-sram #fsmc #access2013-04-19 2:08 AM
Probably because you actually meant :
volatile uint16_t * p_sram_1 = (volatile uint16_t *)0x64000000;
volatile uint16_t * p_sram_2 = (volatile uint16_t *)0x64000002;2013-04-19 3:40 AM
Thank
you
for you
r answer.
What you're saying is
:
Ad
dress 0x6400000
0
points to b
yte 0
Address 0x64000001 points to byte 1
Address 0x6400000
2 points to byte 2
Address 0x64000003 points to byte 3
Since this external SRAM
is connected
to the microcontroller using
a 20-bit address bus, the
memory range is
0x64000000
to 0x640FFFFF,
which means that I can access only 1
MBytes instead of 2MBytes, w
hich is the size of the SRAM
, i
sn't it
?
Whatam I doing wrong
?
2013-04-19 4:02 AM
It's not related to the addressable space.
I mean, the locations your pointers p_sram_1 and p_sram_2 are referring to do overlap. With writing to *p_sram_2, you overwrite one byte of the location where p_sram_1 points to. I believe it is not what you intended to do.2013-04-19 4:11 AM
>
What you're saying is
:
Ad
dress 0x6400000
0
points to b
yte 0
Address 0x64000001 points to byte 1
Address 0x6400000
2 points to byte 2
Address 0x64000003 points to byte 3
Yes.
Since this external SRAMis connected
to the microcontroller using
a 20-bit address bus, the
memory range is
0x64000000
to 0x640FFFFF,
which means that I can access only 1
MBytes instead of 2MBytes, w
hich is the size of the SRAM
, i
sn't it
?
No. The address used in software is byte address, but the address emitted by the FSMC onto address lines is word address. The remaining bit is emitted by hardware as the /UBand /LB byte selection signal (FSMC_BLN0 and FSMC_BLN1). This all provided that the hardware is connected and software configured properly.What
am I doing wrong
?
Y
ou
don't
read the manual carefully enough.
You did not
tell us which model do you use, but
if it is e.g. STM32F4xx, in RM0090 read chapter 32.4.1 NOR/PSRAM address mapping,
especially table 186 and the remark under i
t.
JW
2013-04-19 4:31 AM
Thank you Jan.
Indeed, I missed the chapter 31.4.1in
R
M
0033
which answers my question.By
the way,
I am using
the
STM32F205 model.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.