2017-09-20 6:29 AM
Hi everybody.
I am playing with stm32f411 and external interrupts. I have trouble with interrupt calling in the moment i need. Could you please take a look at my issue?
Id like to call the interrupt by user button pc13. The pin pc13 is pulled up. When the button is pressed, the pin pc13 is connected to the ground (falling edge). But whatever i set on interrupt setting (falling edge/rising edge), the interrupt procedure is called only leaving the button ('unpressing' it) (rising edge).
here i put the setting of the interrupt that i use.
void ext_int_pc13_conf()
{ RCC->APB2ENR |= RCC_APB2ENR_SYSCFGEN; // syscf clk enable RCC->APB2RSTR |= RCC_APB2RSTR_SYSCFGRST;// syscf reset
RCC->APB2RSTR &= ~RCC_APB2RSTR_SYSCFGRST; SYSCFG->EXTICR[3] = SYSCFG_EXTICR4_EXTI13_PC; // pin set as a trigger of ext interrupt EXTI->IMR|
= EXTI_IMR_MR13; // interrupt maskingEXTI->RTSR|
= EXTI_RTSR_TR13; // interrupt trigger on rising edge EXTI->RTSR|
= EXTI_FTSR_TR13; //interrupt trigger on fallingedge
NVIC->IP[EXTI15_10_IRQn] = 0x4; // priority setting NVIC_EnableIRQ(EXTI15_10_IRQn); // interrupt enable return; }Thx for any idea!
js
#pc13 #external-interrupts-button #stm32f411 #stm32f4xx #external-interruptWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.