2017-03-29 3:19 AM
Hi,
I would like to use some external DACs and ADCs connected to my STM32F769 MCU.
The DACs (AD5512) and ADCs (ADS8320) have an interface with :
+ DIN : data input
+ CS : chip select
+ SCLK : clock for the data synchronization
My question is about how to interface with the SCLK signal and what is the best way to implement it. I guess the standard solution is to HIGH or LOW the output pin directly to simulate the clock but I would like to know whether there is another better or more professional solution for doing this using the STM32F7.
Thanks in advanced,
Omar
#dac #stm32f7 #adc2017-03-29 4:17 PM
It appears that both chips could be driven from SPI (clock and data - chipselect still would need to be driven 'manually'), but it's up to you to work out the details.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.