cancel
Showing results for 
Search instead for 
Did you mean: 

EWARM5.20

jilisegiar
Associate II
Posted on July 18, 2008 at 12:42

EWARM5.20

This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15
ettore
Associate II
Posted on May 17, 2011 at 12:39

Hi JJ,

Thank you for the quick reply!

The board was preloaded with the graphical demo, including the ''power-point'' like slides and voice, calendar, ''funny'' etc. I'm able to restore that code using Dfuse and the supplied .dfu images. I just wanted to take the IAR eval board code, build it, generate a .dfu file from the .hex and upload it to the eval board via Dfuse since I don't have a programmer. When my .dfu file is uploaded via Dfuse nothing happens. The screen goes white and the board remains in DFU mode. I can only get the .dfu images supplied with the eval board to work properly. Is there a setting in the linker that I need to change when generating code that will be uploaded via DFU? Thanks in advance!

ettore

jj
Associate II
Posted on May 17, 2011 at 12:39

Arm_Wrestler/Group:

NOW no doubt - you have convinced me! (feared your earlier report

was anecdotal - but it instead springs from ''both'' horses' mouth!)

Suspect that normal/small disty still stock suspect rev's - caveat emptor STM users.

Arm_Wrestler - thanks for sounding this alert - you likely have saved many from avoidable grief. (I am sufficiently challenged JUST trying to make our stuff work - even when all devices/systems are GOOD...)

jj
Associate II
Posted on May 17, 2011 at 12:39

Your detail may have provided a great clue...

Invoke IAR's ''Options'' and insure that ''load code to Flash'' (or similar) is ticked. (on the road now - can't do this for you now & can't precisely recall...)

You're very close - sometimes the last steps are the hardest - keep pushing. Again - be sure you understand boot0/1. Good luck.

jas
Associate II
Posted on May 17, 2011 at 12:39

Hello Guys, the situation so far:

The good news:

The STM32F103VBT6 (100 pin LQFP)devices supplied by Farnell for my production pcb's were rev ''Y'' silicon. :)

http://uk.farnell.com/1447641/semiconductors-integrated-circuits/product.us0?sku=stmicroelectronics-stm32f103vbt6&_requestid=80311

The bad news:

I tried to replace the STM103RBT6 (64 pin LQFP) rev ''B'' device on my IAR STM32-SK dev board with a newer rev ''Y'' device which I ordered from Farnell.

http://uk.farnell.com/1447640/semiconductors-integrated-circuits/product.us0?sku=stmicroelectronics-stm32f103rbt6&_requestid=79321

Unfortunately the replacement chip was a rev ''B'' device also ! :(

So don't assume re-sellers have up to date silicon, Farnell seem to have a mix.

I will have to go through ST sample channels now, I hope it doesn't take too long.

I wan't a working reference design you see, to compare with my production pcb's.

ettore
Associate II
Posted on May 17, 2011 at 12:39

Hi JJ,

I decided to try the Flash Loader demonstrator and that worked perfectly. I'll play with the eval kit like this for now. Thanks for the help!

Ettore

jj
Associate II
Posted on May 17, 2011 at 12:39

A_W-

Thanks your report - indeed disty will ''push'' existing stock - beware...

Would love to learn - if earlier error msg. disappears and if code runs

correctly with your new ''Y'' devices. Wish you success...

One of the STM docs (datasheet/RM0008) identifies exactly where the Rev mark is located. We will likely have to ''feed'' this diagram to disty when ordering parts - to insure that we get recent silicon...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.