2016-10-14 1:06 PM
Hi,
Has someone put the ethernet to work in the F765 or in the F767 microcontrollers, in a custom or development board?Ari.2016-10-28 1:29 AM
Hi mendes.ari.001,
Please note that there was a limitation using RMII on devices Revision A and it was fixed in Revision Z (see for more details).If you aren't in the same conditions as the errata sheet, you need to do farther investigation on your case and keep us informed if you need help.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-10-29 4:16 AM
Thanks Mayla.
Are the revision Z already in production? There will be NUCLEO-F767ZI with revision Z chips? When?Ari.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.