2012-03-29 9:24 AM
The product literature and feature table in the datashee (page 12), all seem to say that Ethernet MAC is only available on 100 pin (and upwards) STM32 F2 devices.
However, looking a bit further down the datasheet, it clearly shows that the ethernet MAC MII and RMII pins are all present on the 64 pin variant! Can someone clarify whether or not any 64 pin STM32 F2 (not F1) devices contain (and can operate with) ethernet MAC or not please? Simon.2012-03-29 10:24 AM
However, looking a bit further down the datasheet, it clearly shows that the ethernet MAC MII and RMII pins are all present on the 64 pin variant!
A bunch of the MII, and several of the RII pins, clearly don't escape on 64 pin parts. Table 6 Only the F207 parts have ethernet, and looking at the Table 3 (pg 13) none of these are in packages below 100 pins.
http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/DATASHEET/CD00237391.pdf
''Ethernet and camera interface available on STM32F207xx devices only.'' STM32F207IC, STM32F207IE, STM32F207IF, STM32F207IG, STM32F207ZC, STM32F207ZE, STM32F207ZF, STM32F207ZG, STM32F207VC, STM32F207VE, STM32F207VF, STM32F207VG2012-03-29 12:36 PM
OK well clearly it's not as clear to some folk as it is to others... ;)
Yes, there are some MII signals that don't come out on the 64 bit part, BUT they are only duplicates so from what I can see the full MII/RMII interfaces (including the serial PHY management interface) is completely present on the 64 bit part. The only down side is that you lose various other peripherals if you use ethernet, but that would suite my application just fine. It would be really good if ethernet works on the 64 pin part. I've been thru the table and extracted the relevent information for ethernet on teh 64 pin devices : 11 MII TX CLK 30 MII TX EN RMII TX EN 33 MII TX D0 RMII TX D0 34 MII TX D1 RMII TX D1 10 MII TX D2 61 MII TX D324 MII RX D0 RMII RX D0
25 MII RX D1 RMII RX D1 26 MII RX D2 27 MII RX D3 29 MII RX ER 23 MII RX DV RMII CRS DV17 MII COL
14 MII CRS 15 MII REF CLK RMII RX CLK9 MDC
16 MDIO I'm new here so I don't know if any ST staff frequent these forums but it would be good to get a definitive answer. Personally I reckon it's the same silicon judging by the pin ordering of the various packages. Simon.From: clive1
Posted: Thursday, March 29, 2012 7:28 PMSubject: Ethernet MAC on 64 pin F2 processorsHowever, looking a bit further down the datasheet, it clearly shows that the ethernet MAC MII and RMII pins are all present on the 64 pin variant!
A bunch of the MII, and several of the RII pins, clearly don't escape on 64 pin parts. Table 6 Only the F207 parts have ethernet, and looking at the Table 3 (pg 13) none of these are in packages below 100 pins.
http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/DATASHEET/CD00237391.pdf
''Ethernet and camera interface available on STM32F207xx devices only.'' STM32F207IC, STM32F207IE, STM32F207IF, STM32F207IG, STM32F207ZC, STM32F207ZE, STM32F207ZF, STM32F207ZG, STM32F207VC, STM32F207VE, STM32F207VF, STM32F207VG2012-03-29 1:46 PM
They are without doubt packaging the same die in different packages. Many of the parts have more memory than specified, and many have peripherals locked out. Whether the 207 die is used elsewhere is something you'll have to discuss with ST.
Your problem however is that there are no STM32F207 or F217 parts in the form factor you seek to use, which part # are you looking at? I'm sure if you're buying $10M+ of parts you might be able to make a deal (ie White Goods Mfg), if not you're probably out of luck. You have a better chance speaking to someone at ST via the usual phone/email of your local ST rep or sales contact.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.