2013-11-13 7:53 AM
Not sure where to file bug reports, but I wanted to make sure this was recorded somewhere.
I've found two errors (so far) in the STM32F30x_StdPeriph_Driver (v1.0.0) that I downloaded to use with the STM32F3-Discovery kit: 1) In stm32f30x_tim.h, in the definition of the TIM_TimeBaseInitTypeDef struct, the TIM_RepetitionCounter field is declared as a uint8_t. This corresponds to the RCR register in the TIM peripheral. This is defined as a uint16_t in stm32f30x.h. Also, according to the technical reference manual, section 16.4.13, the field should be 16-bit. The definition of uint8_t has the effect of limiting the maximum repetition count for no good reason, so I think this is an error. 2) Minor copy/paste error: in the comment for ADC_DMAConfig() in stm32f30x_adc.c the description of the second parameter is wrong (copied from the ADC_DMACmd() function comment directly above it). If this is an appropriate place to post things like this, I might add others that I encounter. If there is a better place, please let me know...2013-11-14 5:08 AM
Hello,
Thanks for reporting, will check your comments. Welcome for your feedbacks. You can continue sending them here. -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2013-11-14 7:01 AM
Agree with you for both comments as TIMx_RCR is 16-bit for TIM1 & TIM8 even if it is 8-bit for TIM15/16/17.
Updates will be applied in coming STandard library release. -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.