2015-08-03 9:05 AM
Hello,
I'm using theSTM32F030R8T6 microcontroller and IAR IDE. The following is a part of code that I'm using:
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1);
/* Configure USART1 pins: Rx and Tx ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_Init(GPIOA, &GPIO_InitStructure);
USART_InitStructure.USART_BaudRate = 38400;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1,ENABLE);
I put:
1.
#ifdef USE_STDPERIPH_DRIVER
2.
#include ''stm32f0xx_conf.h''
3.
#endif /* USE_STDPERIPH_DRIVER */ and in the project configuration i put
STM32F0XX
USE_STDPERIPH_DRIVER
and this is the error:
Error[Li005]: no definition for ''USART_Init'' [referenced from C:\Users\...\Debug\Obj\ filename.o]
Error[Li005]: no definition for ''USART_Cmd'' [referenced from C:\Users\...\Debug\Obj\ filename.o]
Error while running Linker
Can you give me a little help?
2015-08-03 9:15 AM
Can you give me a little help?
You need to add stm32f0xx_usart.c to the files in your project. ie Add an existing file, browse to the directory with the library source in it.Also you should just need to #include ''stm32f0xx.h'', this should pull in the conf.h file based on the define to use the peripheral libray2015-08-03 9:27 AM
Oh my god! You solved my problem in 1 minute! Thank you so much!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.