2015-12-03 11:07 PM
when I try to load code into my STM32F3 discovery board I'm facing the error message Flash download failed-target DLL has been cancelled....I read previous threads also of this same error, I have tried in the following way
1. Jumpered between BOOT0 and VDD 2. Restarted the board 3. In the Debug options selected ''under reset'' and ''auto reset'' options then tried to erase the Flash and tried to load program into flash but again again same error I'm getting please someone help me how can I solve this issue2015-12-04 4:38 AM
Has it ever worked? What where you doing immediately before it stopped working? Do the ST-LINK Utilities work? Do you have multiple contexts of the same IDE open?
Make sure you have current and contemporaneous firmware, drivers and DLLs.2015-12-04 6:13 AM
Hi Clive1,
Yes the board has worked before as i have worked on many peripherals on it. Also even now the the controller is executing the last dumped program perfectly. The only issue is that i am not able to reprogram the device again. Whenever i try to program the device the IDE scolds me with the ''No Target Connected'' as well as ''flash download failed- target DLL has been cancelled ''. I have tried with other board and everything seems to be working fine . Please let me know what can be the issue. Thanks2015-12-04 4:04 PM
Well the primary candidates are, a) reprogramming or interfering with the GPIO pins used by the SWD connection, b) Low Power modes or WFI loops.
2015-12-10 5:01 AM
What are the solutions for these kind of problems?
2015-12-10 8:28 AM
What are the solutions for these kind of problems?
Looking at your code, and not doing those things. It's pretty hard to debug things when you commit those pins to other functions, and remove power from the silicon you're talking too. You could check also the DBGMCU chapter about how you can alter the core behaviour with the debugger.2015-12-24 2:52 AM
I just cleaned my board with the IP then it started working :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.