2015-02-12 2:19 AM
Hi
I have a problem generating a I2C-code for my STM32F2xx.I used the STD_PERIPH_DRIVER and the files it contains. When i compile, i get an error like this: Error[Li005]: no definition for ''assert_param'' [referenced from C:\Users\user\Dropbox\School\Masterproef\Project\I2C-test\Debug\Obj\stm32f2xx_i2c.o] Is there anyone who can help me? Assert_param occurs in a lot of files. I guess i just miss the file that defines the function.Greetings2015-02-12 3:34 AM
You need to add the define ''
USE_STDPERIPH_DRIVER
'' somewhere to your build settings. How you do it depends on your build environment. In case of a makefile, add ''-DUSE_STDPERIPH_DRIVER
''. The ''assert_param()
'' macros is defined in thestm32xxx_conf.h
file, which gets included from thestm32fxxx.h
file - but only ifUSE_STDPERIPH_DRIVER
is defined. (Just assuming the F2xx stdperiph library is designed the same way as those for F0, F1, F3 and F4 ...).We’re moving the ST Community to a new platform to give you a better and more reliable community experience.