2013-11-29 2:53 AM
ES0104: STM32F101xC/D/E and STM32F103xC/D/E high-density device limitations
In CD00197763 �2.13.1 it is statedClear ADDR by reading SR1 register followed by reading SR3SR3? Not SR2? I assume this is an erratum in the errata document? #stm32-i2c-errata-crappy_i2c_core2013-11-29 2:58 AM
The reason I ask is because I get 2 bytes NACK'ed instead of just the last one.
SR1Register = I2C2->SR1;
// If ADDR is set, we cannot read SR2 without clearing ADDR and triggering the
// continuation of the bus access. Instead, we will assume a sensible SR2 value
// (master bit) and defer the reading of SR2 to when we actually want to proceed
SR2Register = (SR1Register & I2C_SR1_ADDR) ? I2C_SR2_MSL : I2C2->SR2;
// If I2C2 is Master (MSL flag = 1)
if
(SR2Register & I2C_SR2_MSL)
{
// If SB = 1, I2C master sent a START on the bus: EV5)
if
(SR1Register & I2C_SR1_SB)
{...
}
else
if
(SR1Register & I2C_SR1_ADDR)
// EV6
{
if
(I2CBus[I2C2BUS].I2CDirection == I2C_Direction_Transmitter)
{...
}
else
// Master Receiver
{
if
(totalSize >2)
{...
}
else
if
(totalSize == 2)
{
// Errata 2.1 EV6_2:
// a) ADDR=1
// b) Override SCL, driving it low
I2C_StretchSCL(I2C2BUS,
true
);
// c) Clear ADDR by reading SR2 after reading SR1
I2C2->SR2;
// d) Program ACK=0
I2C_AcknowledgeConfig(I2C2, DISABLE);
// e) Return SCL control to the I2C core
I2C_StretchSCL(I2C2BUS,
false
);
// We will still get one RxNE interrupt (EV7) after this
When I breakpoint on line 30, the ACK bit is still on. So according to my interpretation of the errata sheet, this should be the way to go.
But on the I2C bus I see the 2 bytes both being NACK'ed?
2013-11-29 3:06 AM
Update: the POS bit needed to be set, then it only nacks the 2nd byte as intended.
I2C_NACKPositionConfig(I2C2, I2C_NACKPosition_Next);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.