2013-06-06 3:37 PM
For DMA_CCRx, halfword and byte write access is broken. In both cases, an interrupt is generated on the instruction following the write instruction. Also, if a byte is written to [15:8], the value is replicated to [7:0].
Here's firmware that reproduces this on STM32F373VCT6-B and STM32F303VCT6-Y:08000188 <
Undefined_Handler
>:
8000188: e7fe b.n 8000188 <
Undefined_Handler
>
800018a: 0000 movs r0, r0
0800018c <
Reset_Handler
>:
// RCC->AHBENR |= RCC_AHBENR_DMA1EN;
800018c: 4b04 ldr r3, [pc, #16] ; (80001a0 <
Reset_Handler
+0x14>)
800018e: 695a ldr r2, [r3, #20]
8000190: f042 0001 orr.w r0, r2, #1
8000194: 6158 str r0, [r3, #20]
// ((__IO uint8_t*)&DMA1_Channel4->CCR)[1] = 0x7A;
8000196: 4b03 ldr r3, [pc, #12] ; (80001a4 <
Reset_Handler
+0x18>)
8000198: 217a movs r1, #122 ; 0x7a
800019a: 7019 strb r1, [r3, #0]
// for (;;) { }
800019c: e7fe b.n 800019c <
Reset_Handler
+0x10>
800019e: bf00 nop
80001a0: 40021000 .word 0x40021000
80001a4: 40020045 .word 0x40020045
The processor ends up in the Undefined_Handler instead of at the for(;;) loop. And the value in
DMA1_Channel4->CCR
is 0x00007A7A (should be 0x00007A00). The workarround is obvious -- only write to DMA_CCRx as 32bit word. -Gary #defect-stm32f32013-06-06 4:42 PM
I suspect there are large tracts of peripheral register space that don't work with partial and/or unaligned write accesses, it's not expected to act like regular RAM with byte lanes, or operate on the same register in some cases (USARTx->DR).
2013-06-06 11:17 PM
Basically true, but if ST writes in RM0313:
10.5 DMA registers
Refer to Section 1.1 on page 36 for a list of abbreviations used in register descriptions. The peripheral registers can be accessed by bytes (8-bit), half-words (16-bit) or words (32-bit). I would assume this to work if stated explicitly. Perhaps an issue of test coverage...2013-06-07 12:02 AM
It appears that the DMA in 'F3xx is the same as in 'F1xx/'L1xx (but different from 'F2xx/'F4xx).
Could anybody please try if this flaw is present in 'F1xx/'L1xx too? JW2013-06-07 12:41 AM
The peripheral registers can be accessed by bytes (8-bit), half-words (16-bit) or words (32-bit).
Maybe they meant that the peripheral registers handled by DMA engine can be 8,16 or 32-bit, not the DMA registers themselves. Who knows.2013-06-07 1:09 AM
No. This refers to the DMA module's registers.
Every ''registers'' subchapter in the UMs starts with describing how these registers can be accessed. The DMA registers subchapter in 'F2/'F4, for example, starts with ''The DMA registers can be accessed by words (32 bits).''. JW2013-06-07 1:23 AM
Maybe they meant that ...
As this is no religious text, but a technical reference manual, there should be no guessing about the ''true meaning''. IMHO a demerit for ST ...
2013-06-07 1:44 AM
No. This refers to the DMA module's registers.
Yes, it is, but who knows where it came from. My guess is that it meant something different originally.Edit: It doesn't look like a hardware bug, definitely documentation problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.