2015-12-08 4:08 AM
Hi
i have seen the below code on this forum. for example if i wnt to make a delay for 10 seconds then how to calculate the tick value.? Can anyone help ?. volatile unsigned int *DWT_CYCCNT = (volatile unsigned int *)0xE0001004; //address of the register volatile unsigned int *DWT_CONTROL = (volatile unsigned int *)0xE0001000; //address of the register volatile unsigned int *SCB_DEMCR = (volatile unsigned int *)0xE000EDFC; //address of the register //****************************************************************************** void EnableTiming(void) { static int enabled = 0; if (!enabled) { *SCB_DEMCR = *SCB_DEMCR | 0x01000000; *DWT_CYCCNT = 0; // reset the counter *DWT_CONTROL = *DWT_CONTROL | 1 ; // enable the counter enabled = 1; } } void TimeDelay(unsigned int tick) { unsigned int start, current; start = *DWT_CYCCNT; do { current = *DWT_CYCCNT; } while((current - start) < tick); }2015-12-08 4:24 AM
10 * HCLK frequency in Hz
But, generally, don't use ''code I have seen'' unless you understand what does it do. JW2015-12-08 4:38 AM
ok.. i understand but not whole.
is it 20160000 for 120ms (168mhz clock)?2015-12-08 4:53 AM
The math here is not unduly complicate, nor the frequency/period relationship
168MHz mean it ticks 168,000,000 times in a second for 120 ms 168,000,000 * 0.120 = 20,160,000 The routine is computing the elapsed time in ~6ns units of time from a free-running 32-bit counter. The 32-bit nature will limit you to about 25.5 seconds in this example. I'm not sure it's entirely appropriate for 10 second delays, but could be modified to implement a timeout. For 10 seconds, it would perhaps be better to use a slower timer and an interrupt so you're not grinding the processor in a loop doing nothing.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.