2018-04-24 2:35 AM
Hello there,
I am using STM32L4 family MCU. I was wondering either it is possible to configure a pin to act as 2 configurations. In my situation, I am trying to make the pin PA0 to act as UART2 CTS line and External interrupt 0. From what I am reading in the datasheet and by checking the way HAL code for initialization is written it should be possible. The problem I am facing however is that my MCU keeps reseting after this config so maybe I am doing something wrong after all. Here is the code generated by MxCube, it configures the pin as uart2 CTS:
/**USART2 GPIO Configuration
PA0 ------> USART2_CTS PA2 ------> USART2_TX PA3 ------> USART2_RX */ GPIO_InitStruct.Pin = GSM_UART2_CTS_Pin|GSM_UART2_TX_Pin|GSM_UART2_RX_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF7_USART2; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);...
HAL_NVIC_SetPriority(USART2_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(USART2_IRQn);// My added code to also enable EXTI:
// Add external interrupt config to UART2 CTS line
GPIO_InitStruct.Pin = GSM_UART2_CTS_Pin; GPIO_InitStruct.Mode |= GPIO_MODE_IT_RISING_FALLING; HAL_GPIO_Init(GSM_UART2_CTS_GPIO_Port, &GPIO_InitStruct); // set IRQ for EXTI0 priority but disable it for now HAL_NVIC_SetPriority(EXTI0_IRQn, 5, 0); HAL_NVIC_EnableIRQ(EXTI0_IRQn);Is there any error in my understanding of this? Is this config a possible one, or do I need to turn CTS off before turning EXTI0 on? I would appreciate all help.
#interrput #uart2018-04-24 2:43 AM
There are certain ways in which a pin might be dual role (e.g. OD output and input at the same time), but alternate function isn't one of them. The second call of HAL_GPIO_Init() discards the previously set alternate function mode for the pin, and only input mode will be functional.
I would recommend simply connecting CTS additionally to a free input pin, which will operate independently as EXTI.
2018-04-24 4:48 AM
Thanks for answer,
Just to be clear about the MCU being reset: MxCube generates code for UART2 CTS and does not for EXTI, so I had no callback defined, thus by going to default callback the MCU reset. After adding the callback manually it works.
As for your answer, are you 100% sure that a pin cannot be alternate function + external interrupt? Because in the HAL_GPIO_Init function there is no 'if - else' statements for configuring the mode. If I make the pin to be alternate + exti, it will configure both, as they do not overlap each other.
External pin tied to UART2 CTS would of course be convenient, but this is a ready design already.
2018-04-24 5:23 AM
The different behavior is provided by the hardware, as the MODER bits are written with different values in each call.
2018-04-24 5:59 AM
Ben,
This time I reversed the initialization order.
The external interrupt 0 works, which would indicate that it was not overlayed with UART2 CTS configuration. Also if I am looking correctly into MODER register, the EXTI config is not configured there.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.