2019-10-23 4:27 AM
We are using STM32F769 NI with DS3231 MZ+ rtc , the rtc is not holding time after a power reset .
The reset pin in the DS3231 circuit is floating , althouigh reset pin has an internal pull up of 50k , can i leave the reset pin floating or should i connect a pull up ?
2019-10-23 4:44 AM
Work together on this, it's not an ST part
https://community.st.com/s/question/0D50X0000BVpH0DSQV/stm32f7-interface-to-ds3231mz
>>can i leave the reset pin floating or should i connect a pull up ?
Couldn't you just add one to the circuit an check that off as an issue?
More likely you don't have the battery wired properly or there is some other issue with the circuit, chip or design
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.