2020-04-09 5:08 AM
in STMCubeMX it says that CAN1 and CAN3 are master and CAN2 is slave. I need to use all three CANs as slave.Would it be possible to do that? If i can do that would i just be configuring the CAN1 and CAN3 as master in STMCubeMX and continue to use them as slaves?
2020-04-14 8:04 AM
Hello @ARam .1
Yes you can use CAN1 and CAN3 as master and continue to us them independently.
Best regards,
Bouraoui
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.