2011-03-04 1:51 PM
Does anyone have any MPU code that just works? STM32F103VG
#mpu2011-05-17 5:26 AM
No - because ''just works'' is meaningless!
You need to specify exactly what ''work'' you want it to do - and in what environment.2011-05-17 5:26 AM
Required MPU basic operation:
1)
Protect a section of RAM.
2)
Access the RAM.
3)
Run the exception routine
My setup is a motor-control application presently utilising timer interrupts, A2D interrupts, and DMA transfers - STM32F103VG, has MPU/has 96kB RAM, all working nicely, except a demo MPU feature:
#define SIZEOF_PROTMEM 0x4000 //16kB;
#define ADDRESS_OF_PROTECTED_SRAM (SRAM_BASE + 0x14000)
volatile __root __no_init u32 au32MyProtectedBuffer[SIZEOF_PROTMEM/sizeof(u32)] @ ADDRESS_OF_PROTECTED_SRAM;
//Disable MPU
MPU_Disable();
//Turn off all regions - the reset states for the ENA bits are undefined.
//No-one else seems to do this – but just for fun OK?
for(u32 u32Rgn=0 ; u32Rgn < ((MPU->TYPE&MPU_TYPE_DREGION_Msk) >> MPU_TYPE_DREGION_Pos) ; u32Rgn++)
{
MPU->RNR = MPU_RNR_REGION_Msk & (u32Rgn << MPU_RNR_REGION_Pos);
MPU->RASR = 0;
};
//
//Configure a no access MPU region for the 16 KB of RAM.
//This region is used for demonstrating an MPU exception.
//
sMPUInit.regionEnable = TRUE;
sMPUInit.regionNo = 0;
sMPUInit.baseAddress = ADDRESS_OF_PROTECTED_SRAM;
sMPUInit.size = mpuRegionSize16Kb;
sMPUInit.accessPermission = mpuRegionNoAccess;
sMPUInit.disableExec = TRUE;
sMPUInit.shareable = FALSE;
sMPUInit.cacheable = TRUE;
sMPUInit.bufferable = TRUE;
sMPUInit.srd = 0xFF;
sMPUInit.tex = 0;
MPU_ConfigureRegion(&sMPUInit);
//Enable the Memory Manage Handler
NVIC_SystemHandlerPriorityConfig(SystemHandler_MemoryManage, 2, 8);
//Enable memory protection and mem fault exceptions – background is Priv-mode open access – courtesy MPU_CTRL_PRIVDEFENA bit.
MPU_Enable(MPU_CTRL_ENABLE_Msk | MPU_CTRL_PRIVDEFENA_Msk);
My trip code:
void SimulateMemoryViolation(void)
{
//Access the forbidden memory!
au32MyProtectedBuffer[0]++;
}
My exception handler which is not being called when I call
SimulateMemoryViolation(),
called from stub inMemManage_Handler():
void EH_MemoryViolation(void)
{
SCB->SHCSR &= ~SCB_SHCSR_MEMFAULTACT; //clear the fault flag
//Go to infinite loop when Memory Manage exception occurs
SetScreen_MPU_Error();
}
Other symptoms: In other variations of this setup (ie. specify code blocks, peripheral blocks, User/Priv permissions etc) I can generate MPU exceptions, or hard faults , but not from accessing my “protected ram.�?
2011-05-17 5:26 AM
As I recall the STM32F103 series doesn't have the MPU included in the M3 core. I believe you have to move the the STM32F200 series for that.
Jack Peacock2011-05-17 5:26 AM
As I recall the STM32F103 series doesn't have the MPU included in the M3 core. I believe you have to move the the STM32F200 series for that.
I think you'll find the STM32F103xF/103xG (ie XL devices) are claiming to have one http://www.datasheetarchive.com/Indexer/Datasheet-099/DSA00188765.html I'd guess I'd start by looking at the code generated for
void SimulateMemoryViolation(void);
2011-05-17 5:26 AM
Oh, great.
Now I see it. The SRD disables the regions if set to 1. Profoundly embarrassed. Anyhow, now it's throwing hardware faults whenSimulateMemoryViolation()
called, not mem-handler exceptions - any observations? Does anyone just have code that ''just works?'' Ta2011-05-17 5:26 AM
OK, so bottom line is, if you invoke an MPU fault from within an exception or interrupt handler, then a hard fault is called. So you must call SimulateMemoryViolation() from the main line.
MPU code that ''just works'' attempt to attach #5.To use the code.
1)
Copy stm32f10x_mpu.c/.h into your StdPeriphLibrary folder.
2)
Copy memprot.c/.h into your project files folder.
3)
Customise memprot.c as required for your ap.
4)
Call
InitMemProt()
frommain()
.5)
Somewhere in your mainline, call
SimulateMemoryViolation()
.6)
In the mem_fault exception handler (in stm32f10x_it.c), place a stub to call
EH_MemoryViolation(),
like this:void MemManage_Handler(void)
{ EH_MemoryViolation(); }7)
Enjoy.
Luke
(may the source be with you)
2011-05-17 5:26 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.