2021-11-27 10:16 PM
I design a stm32h743 board without conformal coating
, it works good, when I shacked board, stm32h743 failed and burnt.
what's that reason?
thank you
Solved! Go to Solution.
2021-11-28 11:32 PM
Independent of coating, every IO of an active component / controller / SoC / whatever should be protected, unless it has some built-in protection (usually only specialized IO drivers), OR the connected circuitry - e.g. a voltage and current limited driver, or an open collector circuit - assures that the maximum ratings cannot be reached.
Protection can be as simple as a small value series resistor, or TVS diodes, ...
I would also recommend to never directly connect a controller pin to the outside world, except for only internally accessible programming / debug pins. Use drivers / receivers, plus protection circuits (and also think about where the surplus energy goes).
2021-11-28 3:46 AM
Voltages and current with value near and above absolute maximum rating will kill the device.
2021-11-28 11:32 PM
Independent of coating, every IO of an active component / controller / SoC / whatever should be protected, unless it has some built-in protection (usually only specialized IO drivers), OR the connected circuitry - e.g. a voltage and current limited driver, or an open collector circuit - assures that the maximum ratings cannot be reached.
Protection can be as simple as a small value series resistor, or TVS diodes, ...
I would also recommend to never directly connect a controller pin to the outside world, except for only internally accessible programming / debug pins. Use drivers / receivers, plus protection circuits (and also think about where the surplus energy goes).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.