2018-05-29 2:32 PM
The documentation for the STM32 F072 is inconsistent:
Section 3.5.4:
'
•
Standby modeThe Standby mode is used to achieve the lowest power consumption. The internal
voltage regulator is switched off so that the entire 1.8 V domain is powered off. The
PLL, the HSI RC and the HSE crystal oscillators are also switched off. After entering
Standby mode, SRAM and register contents are lost except for registers in the RTC
domain and Standby circuitry.
The device exits Standby mode when an external reset (NRST pin), an IWDG reset, a
rising edge on the WKUP pins, or an RTC event occurs.'
Section 6.3.6:
'6.3.6 Wakeup time from low-power mode
The wakeup times given in
Table 36are the latency between the event and the execution of
the first user instruction. The device goes in low-power mode after the WFE (Wait For
Event) instruction, in the case of a WFI (Wait For Interruption) instruction, 16 CPU cycles
must be added to the following timings due to the interrupt latency in the Cortex M0
architecture.
The SYSCLK clock source setting is kept unchanged after wakeup from Sleep mode.
During wakeup from Stop or Standby mode, SYSCLK takes the default setting: HSI 8 MHz.
The wakeup source from Sleep and Stop mode is an EXTI line configured in event mode.
The wakeup source from Standby mode is the WKUP1 pin (PA0).'
My assumption is that the since the part has multiple WKUP pins that any of them can wake up the part from Standby and that Section 6.3.6 is just a carryover from an older part with one WKUP pin, but I would like to know definitely that I can use all of the WKUP pins to come out of standby
2018-05-30 2:37 AM
Hello
Von_Ahnen.Michael
,Measurement in the datasheet were down with this precise WKUP1
but ALL of the
WKUP pins w
ork for Standby mode.
WKUP pins are design precisely to wake up from standby.
With Regards,
Imen.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.