2019-08-23 7:34 AM
I want to use ADC1 and ADC2 in dual mode simultaneous. In reference manual on p.360 there is a note that states that i can't convert tha same channel on both ADCs simultaneously ("no overlapping sampling times for the two ADCs when converting the same channel"). In my case on both ADCs channels 1 and 3 are used, but the channels of ADC1 and ADC2 are (as usual) mapped to different pins. Why can't I convert simultaneously ADC1_CH1 and ADC2_CH2 if these channels are phisically different and each ADC has it's own sampling circuit? Do ADCs have independent input channels in dual mode or share some common set of channels?
2019-08-26 12:42 AM
Hi @RGris
Can you please specify which STM32 you are using ?
Thx
Olivier
2019-08-26 2:24 AM
STM32F303CC
2019-08-26 2:31 AM
Thanks, remove topic "STM32 MPUs" then and add STM32F3.
This should help to reach relevant people for support.
BR
Olivier
2019-08-26 2:41 AM
Olivier as far as I concern this quastion already has topic "STM32F3"
Sould I remove "STM32 MCUs" (not MPU)?
2019-08-26 2:45 AM
No it's ok like this.
STM32 MCUs is parent topic containing STM32F3 but this is to get wider audience for your ticket.
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.