2012-11-28 6:09 AM
Can DMA1 control SDIO and be responsible for transfer data from memory to SD card? I'm using DMA2 for different data transfers. Based on Table 23, page 173, document ID 15403 rev 4 it is not possible because SDIO is mapped to DMA2.
#dma1-sdio2012-11-28 6:50 AM
Assuming STM32F2xx part.
DMA1 is for APB1 peripherals, the SDIO is on APB2. Tables 22 and 23 diagram the DMA request connections.2012-11-28 1:18 PM
Yes it is STM32F2xx.
Thank you clive1.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.