2011-06-04 11:48 AM
Application: Displaying bmp pictures stored on a uSD card.
Board: STM3210E-eval Edit: I've narrowed down the problem. DMA transfer, where the source buffer is SDIO FIFO which must be Word size (32bit), destination is LCD, which must be halfWord(16bit), and memory incriment needs to be disabled for the destination. Basically the first 16bits are transmitted then the rest are lost instead of being sent. How do I fix this? Example code is a couple posts down. (Source can be anything, including SRAM as long as it's set as Word size. So far I have this working fine with SDIO, DMA transfer to SRAM, and then DMA transfer to LCD. But there doesn't seem to be any point in having the SRAM. So I've tried to modfily my program so the information is transfered directly from the SDIO over DMA to the LCD. The problem is the a bit weird. The picture is displayed in a quarter of the screen, with a copy of it next to it. So only half the screen is filled. I tried reading and displaying one sector at a time and that just makes things more confusing. I'm really stuck trying to debug this, i've changed every DMA option to see if any would help... So the main problem I'm having is that I don't know how to start debuging the DMA transfer when memory increment is disabled. Watchpoints don't work...2011-06-04 3:17 PM
seems you have some problems I had. check my post in last week.
I guess it caused by FSMC DMA speed is too slow. try to debug your code if any SD_ERROR happens. In my case, I got SDIO TX_FIFO underrun error when it write data from external memory to SD card with DMA. JZ2011-06-05 10:21 AM
void SD_LCD_DMA_RxConfig(uint16_t *BufferDST, uint32_t BufferSize)
{
DMA_InitTypeDef DMA_InitStructure;
DMA_ClearFlag(DMA2_FLAG_TC4 | DMA2_FLAG_TE4 | DMA2_FLAG_HT4 | DMA2_FLAG_GL4);
/*!< DMA2 Channel4 disable */
DMA_Cmd(DMA2_Channel4, DISABLE);
/*!< DMA2 Channel4
Config
*/DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)SDIO_FIFO_ADDRESS;
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)BufferDST;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
DMA_InitStructure.DMA_BufferSize =0xFFFF;// BufferSize /4; //this doesn't do much
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; //chaning this to half word doesn't fix the problem
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_Init(DMA2_Channel4, &DMA_InitStructure);
DMA_Cmd(DMA2_Channel4, ENABLE);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.