2015-09-30 6:39 AM
Hello,
im using TMS32F071RB. I would like to use USART peripheral in DMA without using interrupt, but polling at TCIF. Is that possible? Thanks, M #dma-usart2015-09-30 9:37 AM
Is that possible?
I would suspect so, I'd probably look at HT and TC, to avoid potential race issues as stuff gets over written, but yes. Might want to work on that dyslexia, it looks like you're using a TI part.2015-09-30 12:03 PM
No reason you have to use an in interrupt as long as there's nothing else for the CPU to do. You may have a problem with variable length incoming messages...how will you know in advance the exact size for the DMA, and what happens if you lose a character or there's a framing/overrun/parity error? A TC loop will spin forever.
For DMA TX no problem since you always know the message length. Jack Peacock2015-10-01 5:03 AM
Frame lenght is going to be constant.
I plan to use LIN mode to recognize EndOfFrame, in case i loose some character.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.