2013-05-27 4:17 AM
Hi, i'm using smt32F303 discovery board, I send / receive data on USART1 without problem if I use interrupt mode, so I think that hardware is good.
I want send a data buffer lenght ~ 8000 bytes using dma mode. Before I config GPIO , USART, and DMA , but on my hyperterminal receive only 4 chars , which is the problem?this is my code:unsigned char tx_buffer[8208];void InitUSART1(void){ GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; USART_InitTypeDef USART_InitStructure; // TX out mode GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOC, &GPIO_InitStructure); // RX in mode GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_Init(GPIOC, &GPIO_InitStructure); /* Connect PXx to USARTx_Tx */ GPIO_PinAFConfig(GPIOC,GPIO_PinSource4,GPIO_AF_7); GPIO_PinAFConfig(GPIOC,GPIO_PinSource5,GPIO_AF_7); /* Interrupt config */ EXTI_InitStructure.EXTI_Line = EXTI_Line25; //usart1 EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); /* Enable and set EXTI0 Interrupt to the lowest priority */ NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x07; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x07; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); USART_InitStructure.USART_BaudRate = 57600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; /* USART configuration */ USART_Init(USART1, &USART_InitStructure); /* interrupt */ USART_ITConfig(USART1,USART_IT_RXNE, ENABLE); /* Enable USART */ USART_Cmd( USART1, ENABLE); /* Enable DMA tx USART */ USART_DMACmd(USART1, USART_DMAReq_Tx, ENABLE); } void SendBufferTx(void){ DMA_InitTypeDef DMA_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); DMA_DeInit(DMA1_Channel4); DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&USART1->TDR; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&tx_buffer; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; DMA_InitStructure.DMA_BufferSize = sizeof(tx_buffer); DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Enable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA1_Channel4, &DMA_InitStructure); DMA_Cmd(DMA1_Channel4, ENABLE); }2013-05-27 4:35 AM
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Enable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
I don't think you need peripheral inc enabled, only memory inc.2013-05-27 4:52 AM
As knik points out the incrementing of the peripheral address (USARTx->DR) is wrong.
This also doesn't do what you expect DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&tx_buffer; Suggest the valid C would be tx_buffer or &tx_buffer[0]2013-05-27 7:17 AM
Thank you for your precious help, now the gaming working properly
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.