2017-10-07 5:12 AM
Hi,
I'm learning about stm32 MCU handling. stm32f0-discovery platform with stm32f072rb MCU.
I have a questions about DMA.
1. How to modify transfer direction? I try to modify DIR bit in CCMR1, but setting is rejected.
2. I have only one DMA1_Channel1->CMAR register. How to achieve memory to memory transfer. I should have two different memory address, source and target.
2017-10-07 6:11 AM
1. There is no CCMR1 register in DMA, you probably meant CCR1? What does 'rejected' mean there? You can't change some (if not all) of DMA_CCRx bits once DMA_CCRx.EN is set.
2. There are two address registers, DMA_CPARx and DMA_CMARx, and their role as source-pointer and destination-pointer swaps with the DMA_CCRx.DIR bit. Don't be misled by the 'peripheral address' name - it's simply an address register and is not aware of whether it points into a peripheral or into other resources, (memories). (This gets different in the more complex DMA module in 'F2/'F4/'F7).
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.