2009-02-04 7:49 PM
DMA Channel Timer1 configuration
2011-05-17 3:56 AM
Hello everyone,
My name is Johann Galea from Malta, and this is my first time in a forum. Right now Im using the STM32F101C. Im trying to convert 7 analogue channels with DMA1, as I will have only one interrupt at the end of the 7 conversions. Im setting the parameters as shown in examples. However, Im not getting a DMA intrerrupt. Timer 1 is working at the desired frequency. Can you please forward any suggestions. These are my codes: void TIM1_UP_IRQHandler(void) { //checks if interrupt occured if (TIM_GetITStatus(TIM1,TIM_IT_Update) == SET) { TIM_ClearITPendingBit(TIM1, TIM_IT_Update); //Start by software the ADC1 Conversion //ADC_Cmd should be called twice, once to wake from powerdown, second to start conversion; manual RM0008 section 10.12.3 ADON not sure ADC_Cmd(ADC1, ENABLE); //enable ADC ADC_Cmd(ADC1, ENABLE); //enable ADC ADC_SoftwareStartConvCmd(ADC1, ENABLE); } void DMA1_Channel1_IRQHandler(void) { //channel 1 includes ADC1 SUPPLY_LED_ON; //this is not turning ON //DMA1_IT_TC1 DMA1 Channel1 transfer complete interrupt //checks wether specified DMA Channel interrupt occured or not. //DMA Channel1 transfer/half complete if (DMA_GetITStatus(DMA1_IT_HT1)==SET) { DMA_ClearITPendingBit(DMA1_IT_HT1);//clear DMA channel transfer complete bit } if(DMA_GetITStatus(DMA1_IT_TC1)==SET) { DMA_ClearITPendingBit(DMA1_IT_TC1);//clear DMA channel1 transfer complete bit } L1v_value = ADC_result[0]; } void Init_ADC(void) { //RM0008 pg 135, low density have DMA1 with 7 channels ADC_InitTypeDef ADC_InitStructure; DMA_InitTypeDef DMA_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; ADC_DeInit(ADC1); //resets ADC1 //Initialisation of DMA channel 1 DMA_DeInit(DMA1_Channel1);//pg 125 DMA_InitStructure.DMA_PeripheralBaseAddr = ADC1_DR_Address;//peripheral base address DMA_InitStructure.DMA_MemoryBaseAddr = (u32)ADC_result;//memory base address DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;//peripheral is the source DMA_InitStructure.DMA_BufferSize = ADC_nbrElement;//number of DMA buffers DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;//peripheral address unchanged DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;//current memory register incremented DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;//16 bits DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;//16 bits DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;//circular buffer mode DMA_InitStructure.DMA_Priority = DMA_Priority_High;//high priority DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;//not from memory to memory transfer DMA_Init(DMA1_Channel1, &DMA_InitStructure); DMA_ClearFlag (DMA1_FLAG_GL1 | DMA1_FLAG_TC1 | DMA1_FLAG_HT1);//clears DMA1 channel 1 transfer complete //Enables DMA channel interrupt when transfer is completed //transfer complete or half complete //DMA_ITConfig( DMA1_Channel1, (DMA1_FLAG_TC1 | DMA1_FLAG_HT1) , ENABLE); /* Enable the DMAChannel1 Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel1_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Enable DMA1 Channel1 complete transfer interrupt */ DMA_ITConfig(DMA1_Channel1, (DMA_IT_TC | DMA_IT_HT), ENABLE); DMA_Cmd(DMA1_Channel1, ENABLE);//enable DMA channel 1 //ADC1 Configuration pg 59 ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;//ADCs operate in independent mode ADC_InitStructure.ADC_ScanConvMode = ENABLE;//conversion done in Scan ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;//only one pass of conversions ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;//conversion started by software ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;//ADC data right aligned ADC_InitStructure.ADC_NbrOfChannel = ADC_nbrElement;//no of ADC channels to convert in a group ADC_Init(ADC1, &ADC_InitStructure); //regular ADC channel configuration ADC_RegularChannelConfig(ADC1, ADC_Channel_0, 1 , ADC_SampleTime_13Cycles5 );//VL1 ADC_RegularChannelConfig(ADC1, ADC_Channel_1, 2 , ADC_SampleTime_13Cycles5 );//VL2 ADC_RegularChannelConfig(ADC1, ADC_Channel_2, 3 , ADC_SampleTime_13Cycles5 );//VT1 ADC_RegularChannelConfig(ADC1, ADC_Channel_3, 4 , ADC_SampleTime_13Cycles5 );//VT2 ADC_RegularChannelConfig(ADC1, ADC_Channel_4, 5 , ADC_SampleTime_13Cycles5 );//VT3 ADC_RegularChannelConfig(ADC1, ADC_Channel_5, 6 , ADC_SampleTime_13Cycles5 );//L3 ref ADC_RegularChannelConfig(ADC1, ADC_Channel_6, 7 , ADC_SampleTime_13Cycles5 );//Shunt ADC_DMACmd(ADC1, ENABLE);//enables ADC1 DMA transfer ADC_Cmd(ADC1, ENABLE); //enable ADC //Resets the selected ADC calibration registers. ADC_ResetCalibration(ADC1); while(ADC_GetResetCalibrationStatus(ADC1)); //start ADC1 calibration ADC_StartCalibration(ADC1); while(ADC_GetCalibrationStatus(ADC1) == SET); } Im suspecting that I have something wrong in the order of the code Many thanks Johann2011-05-17 3:56 AM
Do you set RCC?
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); or Value of ADC_nbrElement ? If it transmited not as ADC_nbrElement, interrupt not generated. Hope help.2011-05-17 3:56 AM
Many thanks. I placed my code on this forum link:
http://www.st.com/mcu/forums-cat-7925-23.html JohannWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.