2008-07-15 3:21 AM
Disable HSI RC when using PLL-HSE as system clock
2011-05-17 3:39 AM
Hey gays,
I'm using the STM3210B-Eval board with IAR EWB and writing my own firmware for better understanding the micro... When I configure the PLL circuit driven by the 8MHz external oszillator (HSE is choosen), can't I turn off the HSI RC part by writing Bit HSION in Register RCC_CR to 0? I'm doing that at the end, when all other clock configurations are done. My debugger runs to memory ''0xFFFFFFFF UNDEFINED INSTRUCTION''... Cheers, Michael2011-05-17 3:39 AM
Ok...solved by setting the correct Flash Latency... (RM0008 page 40)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.