2017-10-26 9:49 AM
Hello,
I am using an STM32F4 MCU and I have a doubt regarding the hardware event .
The datasheet
at section 12.2.3 says'The STM32F4xx are able to handle external or internal events ... '
It's clear for me the interrupt concept but it's not clear to me what is the difference between an hardware interrupt and and hardware event.
Could you clarify it with a simple example ?Thank you in advance.
Regards,
Simon
Solved! Go to Solution.
2017-10-26 10:24 AM
The concept of events in the ARMs is related to interprocessor signalling mainly, so in the standalone Cortex-MXs it's relatively meaningless .
Event input is present in the form of input edge detector (as part of the EXTI module) masked by EXTI_EMR register, and its sole effect is to wake up from WFE-induced sleep.
Event output is present in form of SEV instruction, which outputs a single-cycle pulse on almost all IO pins if set to AF/AF15.
For the most practical purposes you can simply ignore them.
JW
2017-10-26 10:24 AM
The concept of events in the ARMs is related to interprocessor signalling mainly, so in the standalone Cortex-MXs it's relatively meaningless .
Event input is present in the form of input edge detector (as part of the EXTI module) masked by EXTI_EMR register, and its sole effect is to wake up from WFE-induced sleep.
Event output is present in form of SEV instruction, which outputs a single-cycle pulse on almost all IO pins if set to AF/AF15.
For the most practical purposes you can simply ignore them.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.