2016-03-01 8:59 AM
2016-03-14 7:15 AM
Hi kim.young_gil,
VREFINTRDYF (in PWR_CSR register) and VREFINT_RDYF (in SYSCFG_CFGR3 register) are equivalent: both flags are set/reset at the same time and reflect the same state.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-03-20 11:34 PM
Resolution Summary:
SOLUTION PROPOSED BY SUPPORTER - 15/3/2016 07:02:10 :
Dear Both flags are set/reset as the same time and reflects the same state. So, VREFINTRDYF(in PWR_CSR register) and VREFINT_RDYF(in SYSCFG_CFGR3 register) are equivalent. Both flags reflect the state of internal voltage reference in order to provide stable voltage related to analog peripherals And to reduce power consumption in low power mode, it can controlled by EN_VREFINT(in SYSCFG_CFGR3). In additional, ADC, HIS, comparator and temperature sensor have each bit which can independently switch on/off their internal reference voltage. BEst Regards,We’re moving the ST Community to a new platform to give you a better and more reliable community experience.