2008-07-17 10:18 AM
Difference between hardware SDIO and SPI for SD interface?
2011-05-17 3:39 AM
STM32 with 256K flash or above gets hardware SDIO , while 128K or below
using SPI to do SD access! major difference between these 2 access? maximum SD capacity access different? possible compatible issue? support future SD card with larger capacity?2011-05-17 3:39 AM
Hi Kuni,
For SDIO, STM32 High density is fully compatible with SDIO V2.0 and V1.1 and also supports SDHC with larger capacity > 4GBytes and more. Regards, STOne-32.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.