cancel
Showing results for 
Search instead for 
Did you mean: 

DFU for STM32103x

slaven
Associate
Posted on February 02, 2009 at 18:22

DFU for STM32103x

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
slaven
Associate
Posted on May 17, 2011 at 13:01

Hi,

I have a Keil eval board MCBSTM32 (ver 5.1.1) and trying to incorporate DFU. I am able to enter the DFU mode (by using code from STMicro website and implementing necessary mods to the code). I can connect to my PC, recognize the USB devide, installed the driver the first time and able to enter DFU mode. I am also able to create a .DFU file for a simple project. However when I try to download app.dfu, the app gets stuck in erase mode. I get ''Target 00 upgrading - erase phase [22%]''.

I have made sure to change the starting vector address to 0x08003000 and the target and linker options to start the flash address at 0x08003000.

Appreciate any pointers!

Thanks,

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.