cancel
Showing results for 
Search instead for 
Did you mean: 

Development Board for STM32L151CB & STM32L151C8 MCUs

kaljehani
Associate II
Posted on November 27, 2016 at 13:21

Hi, 

We want to develop a LoRa node based on( https://github.com/Lora-net/LoRaMac-node).

They are using STM32L151CB & STM32L151C8 MCUs. 

So, could you please suggest us a development board + all necessary accessories to be able to connect SX1276 to the board and start developing.

Thanks! 
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Posted on November 28, 2016 at 21:52

What facet of those particular parts?

Could you prototype with an L152 NUCLEO or DISCO?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
kaljehani
Associate II
Posted on November 29, 2016 at 11:53

Hi,

I could not understand your first question.

Regarding second one, I did not try any one of them, I am asking for your help to suggest me the best one that matches my requirments. 

I would appreciate any help from any one.

Thanks in advance.

Posted on November 29, 2016 at 17:18

Why are you limited to those specific STM32L1xx parts? I would suggest you do some due diligence work on understanding the code base, and parts used in this project. Discuss with your project supervisor.

http://www.wireless-solutions.de/products/radiomodules/im880b-l.html

http://www.wireless-solutions.de/products/starterkits/sk-im880b.html

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
kaljehani
Associate II
Posted on November 30, 2016 at 06:53

I am following it because I want to be up to date with Semtech's stach implementation. Once they release an updated version of the code, I updated my hardware. 

Note: I have RFM95 LoRa module

Please, if you can suggest me another MCUs that satisfies my needs, I would appreciate it.

Posted on November 30, 2016 at 19:45

I believe the L152 NUCLEO and DISCO boards cited earlier will get the job done, and be an easier port. They have more FLASH/RAM than the part you specified.

It is important that *you* understand the project and its requirements yourself, I don't work for you and this isn't my project, you'll need to do your own homework.

There are no doubt a number of boards you can use to mash-up a working LoRa demonstration.

http://www.ebay.com/itm/SX1276-SX1278-Long-Distance-433MHz-Wireless-Transceiver-Module-LoRa-SPSP-Module-/331962516696?hash=item4d4a8204d8:g:JGwAAOSwZVlXqZ4J

http://www.ebay.com/itm/SX1276-Wireless-LoRa-Module-Semtech-IoT-915MHz-Transceiver-FAST-Ship-SYDNEY-/271693672805?hash=item3f42347165:g:upQAAOSwys5WVQPM

http://forum.modtronix.com/index.php?topic=2197.0

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on February 25, 2018 at 20:22

Clive One wrote:

I believe the L152 NUCLEO and DISCO boards cited earlier will get the job done

Agreed.

In general, you will find that chipmakers cannot provide individual dev boards for each and every possible variant of their entire product range. It is simple not practical.

Instead, they will produce a devboard which is representative of a certain range of products.

So, as

Turvey.Clive.002

‌ says, I think you will find that the

L152 NUCLEO and DISCO boards are representative of the

STM32L151CB & STM32L151C8 parts that you mention.

You can look at the datasheets to determine the precise differences, and whether there is anything critical missing for yourparticular requirements ...

EDIT

There is also this:

http://www.st.com/en/evaluation-tools/b-l072z-lrwan1.html

It contains an STM32L072 (Cortex-M0+) and

SX1276

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.