2024-09-12 11:44 PM
Hello,
I am using RTC internal wake [10 sec] using the following code:
void go_to_sleep(void)
{
HAL_SuspendTick();
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 10, RTC_WAKEUPCLOCK_CK_SPRE_16BITS);
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
SystemClock_Config();
HAL_ResumeTick();
}
After that use following code to detect the source of the wake:
__HAL_RCC_PWR_CLK_ENABLE();
/* Check and Clear the Wakeup flag */
if(__HAL_PWR_GET_FLAG(PWR_FLAG_WUFI) != RESET)
{
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUFI);
printf("RTC Wake Up flag set\n\r");
}
/* Clear source Reset Flag */
__HAL_RCC_CLEAR_RESET_FLAGS();
The device wakes up every 10 seconds and toggles the LED but WUFI is not detected/ set. The RTC is set to WakeUp through Internal WakeUp so I believe WUFI should be set.
Please suggest what could be wrong.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.