2014-02-21 5:16 AM
2014-04-26 5:43 AM
Yes, your project seems to be missing the critical startup_stm32f10x.s (or equivalent) file, describing the STM32F1 interrupt vector table. Please review some of the template projects in the firmware libraries, and use those as a guide to setting up your own.
2014-04-27 10:23 PM
yes. i did not add ''startup_stm32f10x_hd.s'' correctly to my project.
Thanks a lot.2014-06-09 12:05 AM
hi
i have new problem with IAR interrupt. i config TIM2 interrupt and after execute: TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); jtag jump to ''startup_stm32f10x_hd.s'' and stop in line: B TIM2_IRQHandler //---- my config and functions: void TIM2_IRQHandler(void)// call 62.5us Timer INT Lable { if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET) // Qualify the source { TIM_ClearITPendingBit(TIM2, TIM_IT_Update); // Clear the source } if(BufferCounter<(BfrSize-SprtBfrSize)) { if(BufferCounter==0) Buffer_Flag=0x01; DAC_SetDualChannelData(DAC_Align_8b_R,Buffer[BufferCounter],Buffer[BufferCounter]); BufferCounter++; } else { if(BufferCounter==(BfrSize-SprtBfrSize)) Buffer_Flag=0x02; DAC_SetDualChannelData(DAC_Align_8b_R,PBuffer[BufferCounter-(BfrSize-SprtBfrSize)],PBuffer[BufferCounter-(BfrSize-SprtBfrSize)]); BufferCounter++; if(BufferCounter>=BfrSize) BufferCounter=0; } } //---------------------------------- RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);// TIMER2 CLOCK ENABLE RCC_APB1PeriphResetCmd(RCC_APB1Periph_TIM2,DISABLE); NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn; // Define the INT source NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 7;// Define the INT Priority NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;// Enable and Run the Timer NVIC_Init(&NVIC_InitStructure); //------------------- void TIM_Configuration(void)// Timer Config for 10us { TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_TimeBaseStructure.TIM_Period = 4500;//4500 => 62.5us // Timer count to TIM_Period and will be Reset TIM_TimeBaseStructure.TIM_Prescaler = 720; TIM_TimeBaseStructure.TIM_ClockDivision =0; TIM_TimeBaseStructure.TIM_RepetitionCounter=0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;//TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); TIM_ClearITPendingBit(TIM2, TIM_IT_Update); // Clear the source TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); TIM_Cmd(TIM2, ENABLE); }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.