2012-08-29 2:22 AM
I use this command DBGMCU_Config(DBGMCU_IWDG_STOP, ENABLE);
I added &sharpinclude ''stm32f10x_dbgmcu.h'' in the include list.I also see stm32f10x_dbgmcu.h in STD Library.But it's not working !I get a linker error:no definition for ''DBGMCU_Config''Error while running Linker The compiler is IAR ver 6.10What shuld I do in order to solve this problem ?Thanks
Yaniv #dbgmcu_config2012-08-29 2:53 AM
I use this command DBGMCU_Config(DBGMCU_IWDG_STOP, ENABLE);
It is not a command, but a function you call.I added #include ''stm32f10x_dbgmcu.h'' in the include list.
...
But it's not working !
I get a linker error:
That's normal. You need to add the implementation of this function, too. This is in ''stm32f10x_dbgmcu.c''. Add this file to your project, and it should work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.