2017-04-01 4:02 AM
Hello Everyone,
Does anyone know a module for I2S DAC ?
Thanks
#stm32f1xxx #i2s #dac2017-04-01 4:46 PM
How can I interface this board to STM32 ?
From datasheet for I2S, what's the relation with the board ?
The SPI could function as an audio I2S interface when the I2S capability is enabled (by
setting the I2SMOD bit in the SPI_I2SCFGR register). This interface uses almost the samepins, flags and interrupts as the SPI.The I2S shares three common pins with the SPI:â—� SD: Serial Data (mapped on the MOSI pin) to transmit or receive the two timemultiplexeddata channels (in simplex mode only).â—� WS: Word Select (mapped on the NSS pin) is the data control signal output in mastermode and input in slave mode.â—� CK: Serial Clock (mapped on the SCK pin) is the serial clock output in master modeand serial clock input in slave mode.An additional pin could be used when a master clock output is needed for some externalaudio devices:â—� MCK: Master Clock (mapped separately) is used, when the I2S is configured in mastermode (and when the MCKOE bit in the SPI_I2SPR register is set), to output thisadditional clock generated at a preconfigured frequency rate equal to 256 × FS, whereFS is the audio sampling frequency.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.