2015-06-08 1:45 AM
Dear all,
I've notice an ennoying bug in new version of CubeMX when generating project for MDKARMv5 based on STM32L152RBT6 MCU : The generated project define both ''STM32L152xB'' and ''STM32L152xBA'' preprocessor symbols in the toolchain configuration. This induces re-definition conflict in the file ''stm32l1xx_hal_flash_ex.h'' wich totally mess-up the project when cimpiling. Removing STM32L152xBA in symbols list solve the problem, but must be done each time you update the project from CubeMX. I've not noticed this problem with previous version of CubeMX (last used version was 4.5). Thank you for fixing this issue as soon as possible. BaDuf2015-06-18 5:14 AM
Hi,
I reproduced the issue and I confirm the re-definition error.2015-06-18 6:40 AM
Hello,
Thanks for reporting this issue.It will be fixed in coming CubeMX release.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-06-24 8:49 AM
Hi Mayla,
Thank you for this information ! Nothing related but, is there a specific way for reporting bug (such as a ''bugtracker'') instead of posting on the forum ? It should help to follow status of the bug and which version of Cube should be used to have a fix. Thank youWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.