2015-12-21 3:51 AM
I tried to generate code for STM32F407VG using cubemx[4.12] with following settings for STM32F4-Discovery.
- RCC - High Speed Clock(HSE) –Crystal/Ceramic Resonator, - USB_OTG_FS – Mode [Host Only ] & Activate_Vbus [ticked], - USART6 – Mode [Asynchronous] - FATFS –USBDisk[ticked], - USBHOST-Class for FS IP [Mass storage Host class] - GPIO - PC0- GPIOOutput - Clock - 8Mhz HSE, HCLK 168Mhz, PLL M(4), N(168), P(2), Q(7) - USB_HOST-Platform settings- Supported Ips [Gpio output] Found solutions[pc0]Attached here .ioc project file and modified main.c is listed below. The program fails in f_open call after passing through f_mount call. Increasing of stack and heap size did not help.
Any solution or clue would be useful.---------
Listing of modified main.c #include ''stm32f4xx_hal.h'' #include ''fatfs.h'' #include ''usb_host.h''UART_HandleTypeDef huart6;
FATFS USBDISKFatFs; FIL MyFile; extern ApplicationTypeDef Appli_state; char USB_Path[4];void SystemClock_Config(void);
static void MX_GPIO_Init(void); static void MX_USART6_UART_Init(void); void MX_USB_HOST_Process(void);/** System Clock Configuration
*/ void SystemClock_Config(void) {RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;__PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 4; RCC_OscInitStruct.PLL.PLLN = 168; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 7; HAL_RCC_OscConfig(&RCC_OscInitStruct);RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1
|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2; HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5);HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0); }/* USART6 init function */
void MX_USART6_UART_Init(void){huart6.Instance = USART6;
huart6.Init.BaudRate = 115200; huart6.Init.WordLength = UART_WORDLENGTH_8B; huart6.Init.StopBits = UART_STOPBITS_1; huart6.Init.Parity = UART_PARITY_NONE; huart6.Init.Mode = UART_MODE_TX_RX; huart6.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart6.Init.OverSampling = UART_OVERSAMPLING_16; HAL_UART_Init(&huart6);}
void MX_GPIO_Init(void) {GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__GPIOH_CLK_ENABLE(); __GPIOC_CLK_ENABLE(); __GPIOA_CLK_ENABLE();/*Configure GPIO pin : PC0 */
GPIO_InitStruct.Pin = GPIO_PIN_0; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_LOW; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);}
//============================================================================
#define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f) //----------------------------------------------------------------------------- PUTCHAR_PROTOTYPE { HAL_UART_Transmit(&huart6, (uint8_t*)&ch, 1, 5); return ch; } //----------------------------------------------------------------------------- static void Error_Handler(void){ printf(''error....\r\n''); while(1) { } } //----------------------------------------------------------------------------- #ifdef USE_FULL_ASSERT void assert_failed(uint8_t* file, uint32_t line){ while (1) { }} #endif //----------------------------------------------------------------------------- static void MSC_Application(void){ FRESULT res; uint32_t byteswritten; uint8_t wtext[] = ''This is STM32 working with FatFs''; printf(''in MSC_Application ...usbh path %s \r\n'',USBH_Path); if(f_mount(&USBDISKFatFs, (TCHAR const*)USB_Path, 0) != FR_OK) {printf(''f_mount fail ...\r\n''); Error_Handler();}/* FatFs Initialization Error */ else{ printf(''mount ok...\r\n''); if(f_open(&MyFile, ''STM32.TXT'', FA_CREATE_ALWAYS | FA_WRITE) != FR_OK){ printf(''f_open fail \r\n'');Error_Handler(); } else{ printf(''f_write ...\r\n''); res = f_write(&MyFile, wtext, sizeof(wtext), (void *)&byteswritten); if((byteswritten == 0) || (res != FR_OK)) { Error_Handler(); } else { f_close(&MyFile); printf(''success....\r\n'');} } } } } //----------------------------------------------------------------------------- int main(void){ HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); MX_USART6_UART_Init(); HAL_UART_MspInit(&huart6); MX_FATFS_Init(); MX_USB_HOST_Init(); while (1) { MX_USB_HOST_Process(); switch(Appli_state) { case APPLICATION_START: MSC_Application(); Appli_state = APPLICATION_IDLE; break; case APPLICATION_IDLE: default: break; } } }//------------------------------------------------
2016-08-08 9:27 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.