2021-03-05 4:47 PM
I recently upgraded my CubeIDE installation from 1.5 to 1.6.
Is it necessary to use the 1.5 which came with the workshop-material or does it also work with the newer 1.6?
Thank you for your answer.
Best regards
2021-03-08 9:36 AM
Hello,
I would recommend using 1.5 if possible, since this one was tested for the hands-on examples. In general, it should work on v1.6, but there could be some catch.
Best regards,
Adam Berlinger
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.