cancel
Showing results for 
Search instead for 
Did you mean: 

Cube V1.1.1: Why is TIM_CCxNChannelCmd private?

andywild2
Associate III
Posted on December 23, 2015 at 09:04

Hello,

I use the STM32F2xx.

I need to enable TIM8 OCN Output.

I cannot do that because TIM_CCxNChannelCmd is private.

Second issue with ADC:

If I set ExternalTrigConv = ADC_SOFTWARE_START;

in this case the parameter ExternalTrigConvEdge is don´t care.

However HAL_ADC_Start() checks the ExternalTrigConvEdge parameter for correct values!! and does not check ExternalTrigConv first!

So the user HAS TO init ExternalTrigConvEdge otherwise HAL_ADC_Start() might throw an error with parameter checking.

Will this be fixed in the next release?

best regards

Andy
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.