2017-04-03 12:22 PM
I dont have much of a problem using the examples, but I do have a problem if I try to use ioc/cube generated samples that I try to retro fit in example code from the discovery repot.
In particular, the touch middleware is not provided by the cube software so I have to hand fit in the code from the example and then try to fix the gazillion errors. Well not a gazillion, but 310 errors.
Its not easy problem to solve with the headers included in headers.
2017-04-04 1:16 AM
Hi
Davis.John.004
,Your description of the issue is general.
You should identify what is the problem that you see and when it occurs.
Formore understand the issue you are facing, you can share your .ioc/code file and precisewhich device, firmware and CubeMx version you have used.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.