2011-07-11 6:01 AM
I'm an absolutly beginner in microcontrollers.
I want to create a simple square wave signal on STM32F103VB with tim3, ch2, but nothing happens. Can anybody tell me what I'm doing wrong? Thanks Tom #define DEF_SPEED 140; #define CCR1_Val 32768; int main(void) { GPIO_InitTypeDef GPIO_InitStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; // RCC/System clocks configuration RCC_Config(); // Enable Timer3 clock and release reset RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE); // map PC7 as TIM3-CH2 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; //7 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; // clock to 50MHz GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; // alternate function pull GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_PinRemapConfig(GPIO_FullRemap_TIM3, ENABLE); // ?!!!!!!!!!! // Time base configuration TIM_TimeBaseStructure.TIM_Period = 0xFF; // 8 bit resolution TIM_TimeBaseStructure.TIM_Prescaler = DEF_SPEED; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); // Output Compare Toggle Mode configuration: Channel2 TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle; TIM_OCInitStructure.TIM_Pulse = CCR1_Val; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low; TIM_OC2Init(TIM3, &TIM_OCInitStructure); TIM_Cmd(TIM3,ENABLE); while (1) {} }2014-06-05 8:57 AM
2014-06-05 9:13 AM
What board and chip are we talking about here? If it's an F100 on a VL-Discovery double check if the chip supports the specific timers
What other output do you see from your program? Do you see output from the non-remapped pins? You might need to change the JTAG remapping /* Disable the Serial Wire Jtag Debug Port SWJ-DP */ GPIO_PinRemapConfig(GPIO_Remap_SWJ_Disable, ENABLE); or /* JTAG-DP Disabled and SW-DP Enabled */ GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE);2014-06-05 9:35 AM
Sorry i forgot to mention im using STM32F100 Discovery board. I tried using TIM3 full remapping and i was able to get blinking LED (PC9). I thought it might be something to do with CH4 as PC9 is on CH4. With TIM3 partial remapping I was also able to get a pwm on PB1 which again is CH4. If I try to get the output on CH2 (TIM2) or CH1 (TIM3) I dont get the output.
2014-06-05 10:09 AM
/* Dual PWM Remap Demo PB3/PB4 - STM32 VL-Discovery - sourcer32@gmail.com */
#include ''stm32F10x.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
// clock for GPIO and AFIO (REMAP)
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO, ENABLE);
// clock for TIM2 and TIM3
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2 | RCC_APB1Periph_TIM3, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
// PB3 TIM2_CH2
// PB4 TIM3_CH1
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3 | GPIO_Pin_4;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_PinRemapConfig(GPIO_FullRemap_TIM2, ENABLE); // Remapped to CH2 PB3
GPIO_PinRemapConfig(GPIO_PartialRemap_TIM3, ENABLE); // Remapped to CH1 PB4
/* JTAG-DP Disabled and SW-DP Enabled */
GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE); // Off PB3/PB4 - REQUIRED
}
/**************************************************************************************/
void TIM2_Configuration(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
TIM_TimeBaseStructure.TIM_Prescaler = (SystemCoreClock / 1000000) - 1; // 1 MHz
TIM_TimeBaseStructure.TIM_Period = 500 - 1; // 1 MHz / 500 = 2 KHz
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
// Channel 2 configuration = PB.03 TIM2_CH2
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = (TIM_TimeBaseStructure.TIM_Period + 1) / 2; // 50% Duty
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC2Init(TIM2, &TIM_OCInitStructure);
// turning on TIM2 and PWM outputs
TIM_Cmd(TIM2, ENABLE);
}
/**************************************************************************************/
void TIM3_Configuration(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
TIM_TimeBaseStructure.TIM_Prescaler = (SystemCoreClock / 1000000) - 1; // 1 MHz
TIM_TimeBaseStructure.TIM_Period = 250 - 1; // 1 MHz / 250 = 2 KHz
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
// Channel 1 configuration = PB.04 TIM3_CH1
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = (TIM_TimeBaseStructure.TIM_Period + 1) / 4; // 25% Duty
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC1Init(TIM3, &TIM_OCInitStructure);
// turning on TIM3 and PWM outputs
TIM_Cmd(TIM3, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
TIM2_Configuration();
TIM3_Configuration();
while(1);
}
/**************************************************************************************/
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d
'', file, line) */
/* Infinite loop */
while (1)
{
}
}
#endif
2014-06-05 10:19 AM
Thank you clive1! I will try this now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.